This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SN65HVD1792-EP: sn65hvd1792-ep とsn65hvd1792の違いについて

Part Number: SN65HVD1792-EP

sn65hvd1792TDEPとSN65HVD1792D

は、データシート上、同じスペックのようなのですが、型番の違いでの異なる点は何になりますでしょうか。

  • "-EP" means "enhanced product". The Enhanced Product Selection Guide says:

    Our enhanced products portfolio mitigates the risks that the avionics and defense markets face with COTS integrated circuits (ICs) by:

    • Using the latest and most robust plastic encapsulation methodology to support the harsh environment needs.
    • Ensuring tin plating content is not above 97% to eliminate the risks related to time-dependent pin-to-pin metal shorts (aka tin whiskers) by assembling the device with NiPdAu plating or SnPb solder balls.
    • Using only gold (Au) bond wires to ensure the highest quality die to leadframe connection.
    • Performing extended 250 hours highly accelerated temperature and humidity stress testing (HAST) to demonstrate improved moisture resistance, extending both operational life and dormant storage capabilities.
    • Extending temperature ranges from -55°C to 125°C to enable the broadest possible use cases.
    • Ensuring a single controlled manufacturing baseline flow with a single wafer fab, assembly site and test site to ensure the applicability of customer’s qualification even over multi-decade programs.
    • Ensuring orderable (V62/xxxx) DLA vendor items drawings part numbers that eliminate the need specification source controlled drawings.