Part Number: DS90UB926Q-Q1
Hello,
I would like to confirm that writing register 0x07 will set the remote serializer I2C Device ID. Currently the remote serializer (DS90UB921) ID is set by its IDx pin.
I have a desire to override the IDx pin setting and am hoping I can do so by writing a new Device ID to register 0x07 on the local deserializer. It appears I also need to set bit 0 to a '1' to prevent it from changing back.
Below is the register description from the DS90UB926Q1 data sheet.
Thanks.