Part Number: TCA9617A
Other Parts Discussed in Thread: TCA39306, PCA9306, TCA9406
Hi, Expert
my customer want to use TCA9617 as a level shifter between MAC and PHY, interface is MDIO, could it support MDIO?
BR
Chi
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Chi,
What speed are you running your MDIO signal at. Typically MDIO speeds are much faster than I2C speeds and most likely the TCA9617 would not be able to achieve that speed.
We have a device called the PCA9306/TCA39306 which does support MDIO but under specific conditions. What voltages levels are you trying to translate between, and do you need a buffer?
Best,
Chris
Hi, Chris
thanks for your feedback.
my customer want 1.8V-3.3V 2.5MHz MDIO signal, so we will choose PCA9306 device.
also, I have take your https://e2e.ti.com/support/interface/f/138/t/584378 as reference.
BR
Chi
Chi,
That is good to hear let me know how it goes. One thing to look out for is what high level you will be able to achieve with your clock speed. You will have to balance high VOLs with slow rise time. With a speed this fast you will have to use strong pull ups in order to have fast rise times but this will hurt your VOLs.
Another device that can work out here at a speed of 2.5MHz can also be the TCA9406. This device comes with a rise time accelerator and it's own internal pull ups. You can attach additional external pull up resistors. This device can achieve 2 Mbps with open drain driving and 21 Mbps for push pull driving. But this assumes a low capacitive load and an output impedance of your external driver of 50 ohms. This device was not tested with MDIO like the PCA9306 but it can potentially work and might be something else to look at.
Best,
Chris