Part Number: TPD3S713-Q1
Hi team,
I plan to connect IMON output to ADC in MCU(3.3V).
RILIM=6.98kohm, RIMON=5.6kohm
Since MCU input tolerance is 3.3V, I need to limit the VMON voltage less than 3.3V.
I concerns the voltage spike caused by inrush current to VBUS might violate 3.3V output.
Could you advise below?
1. How does IMON output behave when large inrush current flows? It is described that high current flaws for 1 to 2us(typical) before current limit circuit react in the datasheet?
2. Should I use clamp diode externally?
3. How much is the current limit (maximum current) out from IMON?
regards,