Part Number: DS125BR800
Hi,
I'm having trouble using the IBIS-AMI model in an ADS simulation.
I get the following error when starting a simulation using the IBIS model including the example project:
Error detected by hpeesofsim in DS125BRxxx_Rx_AMI during netlist flattening.
Unable to load AMI library '/localstore/basvdh/ads_proj/ibis/TI_DS125BR800_IBIS_AMI_v2/Example_Projects/Agilent_ADS_2011.10/data/DS125BRxxx_Rx_11_2012_x64.so'.
Please check in your IBIS file whether AMI library (DLL)
for the 64-bit Linux platform is specified and
whether it is stored in the same folder as the IBIS file.
Linker Error: '/localstore/basvdh/ads_proj/ibis/TI_DS125BR800_IBIS_AMI_v2/Example_Projects/Agilent_ADS_2011.10/data/DS125BRxxx_Rx_11_2012_x64.so: undefined symbol: s_Fini'
I'm not sure how to fix this as I can't find anything this s_Fini library?
I'm using ADS 2022.1 on Redhat 8.6
Thanks in advance.
Regards,
Bas.