Part Number: DP83867E
Other Parts Discussed in Thread: DP83869HM
Dear team,
Customer is planning to use the DP83867 (or DP83869HM) and they would like to make sure both Ethernet phy are compatible with 100Base-TX and 1000-Base-T using the same PCB (4 pairs routed for ethernet).
The PHY would be addressed in RGMII.
From what I understood by going through the datasheet and the e2e:
- The PHY can be used in 100Base-TX when addressed in RGMII
- The PHY uses channels A and B only when in 100Base-T mode (C & D are not used). In 1000Base-T, the 4 channels are used.
- The configuration of the 100Base-T or 1000Base-T PHY is done internally via registers (in particular the 0x0000 register)
Could you please confirm that the points above would be covered by the DP83867 and DP83869HM?
Thanks in advance for your feedback.
Regards,
Pol.