Part Number: DS90C241
Other Parts Discussed in Thread: DS90C124
Hi,
I am planning to use the Serdes pair DS90c124 and DS90c241 in a design.
I use the serializer to serialize 24 signals (max frequency signal 10 MHz) and send them across a 5 meter CAT5e cable to the Auxiliary board.
The boards are powered by separate 24V SMPS.
I need your help to understand whether the "24V Digital Ground" should be made common between the two boards or kept isolated.
Since the only interface between these 2 boards is the differential pair, I feel this must not be required.
ON my research on the internet, I have seen some people suggesting isolating the two power supplies, and some people suggest that making the ground common is not required.
Please suggest.