Part Number: TUSB1310
Hi,
We are using add on board from E-Elements which is based on TUSB1310 chip.
We are testing USB 3.0 Host controller solution.
TX_DETRX_LPBK is getting asserted from Host controller side.
In response PHY_STATUS is getting asserted.
In response {RX_STATUS2,RX_STATUS1,RX_STATUS0} is always 0.
The response we are expecting - {RX_STATUS2,RX_STATUS1,RX_STATUS0] should be 11 when PHY_STATUS is getting asserted for TX_DETRX_LPBK assertion.
Please help us on why { RX_STATUS2,RX_STATUS1,RX_STATUS0} is continuously 0 instead of 11 for TX_DETRX_LPBK assertion.
Regards
Sampath