Other Parts Discussed in Thread: TFP403, TFP401A
can we use TFP101 for resolution up to (1280x800), and what is the best and largest resolution fot TFP101??please help me
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello Hendri, sorry for the delayed response.
TI's DVI devices are ignorant to the resolution, and only care about the pixel frequency. So any resolution + refresh rate that's between 25-86MHz is supported.
There's a VESA doc labeled "VESA and Industry Standards and Guidelines for Computer Display Monitor Timing (DMT)" with tables of resolutions+refresh and their associated pixel clocks. There's also a free Excel-based CVT calculator that you can download from VESA after you register (or a google search reveals it's available here). The calculator result doesn't always perfectly match the DMT tables.
To answer your question about 1280x800, the DMT table for 60Hz reduced-blanking has 71MHz, and 60Hz regular-blanking is 83.5MHz. 1366x768 at 60Hz_reduced is 72MHz, and at 60Hz_regular is 85.5MHz. All of these are <86MHz and are supported.
Note that the TFP401A or TFP403 are strongly recommended for new designs, rather than the TFP101.
Thanks,
RE