Part Number: DS90UB949A-Q1EVM
Other Parts Discussed in Thread: ALP
Hello everyone,
I am having a DS90UB949A-Q1EVM Serializer kit which is connected to the Deserializer using an FPD Link cable. I have gone through the Serializer EVM kit manual and did the Jumper settings as described in the manual. For reference, I am mentioning the settings of IDx: #2, MODE_SEL0: #1, and MODE_SEL1: #5, I am having an external EEPROM that contains the EDID data bytes.
The setup includes a Serializer, a Deserializer, a Laptop, and a Touch Display device. The laptop is connected to the Serializer using an HDMI cable while the Touch Display device is connected to the Deser side. The problem is that once I connect the HDMI cable to the laptop which is the display source, then the Serializer is unable to forward the display of the Laptop screen to the Touch Screen display. While some of the laptops are working fine but some laptops are not able to detect the Serializer as a Display device/monitor. All the laptops are running Windows 10 and Windows 11.
The HPD pins are asserted when I connect the HDMI cable to the laptop but still, no display is forwarded on the Touch display screen.
I am attaching the register dump of Ser and Deser collected using ALP Tool provided by the TI. These register dumps are collected from the laptop in which the screen is not forwarded.
[REGISTERS] Device = ALP Nano 1 - DS90UB949, Connector 1 Comments = "Ser Device Data" Date = 07/08/2022 Time = 19:16:32 Reg = 0,0x0000,0x1C Reg = 0,0x0001,0x00 Reg = 0,0x0003,0xDA Reg = 0,0x0004,0x80 Reg = 0,0x0005,0x00 Reg = 0,0x0006,0x58 Reg = 0,0x0007,0x00 Reg = 0,0x0008,0x00 Reg = 0,0x0009,0x00 Reg = 0,0x000A,0x11 Reg = 0,0x000B,0x00 Reg = 0,0x000C,0x03 Reg = 0,0x000D,0x20 Reg = 0,0x000E,0x00 Reg = 0,0x000F,0x00 Reg = 0,0x0010,0x00 Reg = 0,0x0011,0x00 Reg = 0,0x0012,0x00 Reg = 0,0x0013,0x8C Reg = 0,0x0014,0x00 Reg = 0,0x0015,0x01 Reg = 0,0x0016,0xFE Reg = 0,0x0017,0x1E Reg = 0,0x0018,0x7F Reg = 0,0x0019,0x7F Reg = 0,0x001A,0x01 Reg = 0,0x001B,0x00 Reg = 0,0x001C,0x00 Reg = 0,0x001D,0x00 Reg = 0,0x001E,0x05 Reg = 0,0x001F,0xF6 Reg = 0,0x0020,0x0B Reg = 0,0x0021,0x00 Reg = 0,0x0022,0x25 Reg = 0,0x0023,0x00 Reg = 0,0x0024,0x00 Reg = 0,0x0025,0x00 Reg = 0,0x0026,0x00 Reg = 0,0x0027,0x00 Reg = 0,0x0028,0x01 Reg = 0,0x0029,0x20 Reg = 0,0x002A,0x20 Reg = 0,0x002B,0xA0 Reg = 0,0x002C,0x00 Reg = 0,0x0030,0x00 Reg = 0,0x0031,0x00 Reg = 0,0x0032,0x00 Reg = 0,0x0033,0x00 Reg = 0,0x0034,0x00 Reg = 0,0x0035,0x00 Reg = 0,0x0036,0x00 Reg = 0,0x0037,0x00 Reg = 0,0x0038,0x00 Reg = 0,0x0039,0x00 Reg = 0,0x003A,0x00 Reg = 0,0x003B,0x00 Reg = 0,0x003C,0x00 Reg = 0,0x003D,0x00 Reg = 0,0x003E,0x00 Reg = 0,0x003F,0x00 Reg = 0,0x0040,0x14 Reg = 0,0x0041,0x55 Reg = 0,0x0042,0x00 Reg = 0,0x0043,0x00 Reg = 0,0x0044,0x80 Reg = 0,0x0045,0x00 Reg = 0,0x0046,0x00 Reg = 0,0x0047,0x00 Reg = 0,0x0048,0x01 Reg = 0,0x0049,0x68 Reg = 0,0x004A,0x01 Reg = 0,0x004B,0x00 Reg = 0,0x004C,0x00 Reg = 0,0x004D,0x00 Reg = 0,0x004E,0x00 Reg = 0,0x004F,0x01 Reg = 0,0x0050,0x97 Reg = 0,0x0051,0xA1 Reg = 0,0x0052,0x1E Reg = 0,0x0053,0x00 Reg = 0,0x0054,0x28 Reg = 0,0x0055,0x0C Reg = 0,0x0056,0x00 Reg = 0,0x0057,0x00 Reg = 0,0x0058,0x00 Reg = 0,0x0059,0x00 Reg = 0,0x005A,0x92 Reg = 0,0x005B,0x20 Reg = 0,0x005C,0x02 Reg = 0,0x005D,0x06 Reg = 0,0x005E,0x44 Reg = 0,0x005F,0x00 Reg = 0,0x0060,0x22 Reg = 0,0x0061,0x02 Reg = 0,0x0062,0x00 Reg = 0,0x0064,0x10 Reg = 0,0x0065,0x00 Reg = 0,0x0066,0x00 Reg = 0,0x0067,0x00 Reg = 0,0x0068,0x00 Reg = 0,0x0069,0x00 Reg = 0,0x006A,0x00 Reg = 0,0x006B,0x00 Reg = 0,0x006C,0x00 Reg = 0,0x0070,0x00 Reg = 0,0x0071,0x00 Reg = 0,0x0072,0x00 Reg = 0,0x0073,0x00 Reg = 0,0x0074,0x00 Reg = 0,0x0075,0x00 Reg = 0,0x0076,0x00 Reg = 0,0x0077,0x00 Reg = 0,0x0078,0x00 Reg = 0,0x0079,0x00 Reg = 0,0x007A,0x00 Reg = 0,0x007B,0x00 Reg = 0,0x007C,0x00 Reg = 0,0x007D,0x00 Reg = 0,0x0080,0x00 Reg = 0,0x0081,0x00 Reg = 0,0x0082,0x00 Reg = 0,0x0083,0x00 Reg = 0,0x0084,0x00 Reg = 0,0x0090,0x00 Reg = 0,0x0091,0x00 Reg = 0,0x0092,0x00 Reg = 0,0x0093,0x00 Reg = 0,0x0094,0x00 Reg = 0,0x0098,0x00 Reg = 0,0x0099,0x00 Reg = 0,0x009A,0x00 Reg = 0,0x009B,0x00 Reg = 0,0x009C,0x00 Reg = 0,0x009D,0x00 Reg = 0,0x009E,0x00 Reg = 0,0x009F,0x00 Reg = 0,0x00A0,0x00 Reg = 0,0x00A1,0x00 Reg = 0,0x00A2,0x00 Reg = 0,0x00A3,0x00 Reg = 0,0x00C0,0x00 Reg = 0,0x00C1,0x00 Reg = 0,0x00C2,0xA8 Reg = 0,0x00C3,0x00 Reg = 0,0x00C4,0x28 Reg = 0,0x00C5,0x00 Reg = 0,0x00C6,0x00 Reg = 0,0x00C7,0x60 Reg = 0,0x00C8,0xC0 Reg = 0,0x00C9,0x00 Reg = 0,0x00CA,0x00 Reg = 0,0x00CB,0x00 Reg = 0,0x00CC,0x00 Reg = 0,0x00CE,0xFF Reg = 0,0x00D0,0x00 Reg = 0,0x00D1,0x00 Reg = 0,0x00D2,0x00 Reg = 0,0x00D3,0x00 Reg = 0,0x00E0,0x00 Reg = 0,0x00E1,0x00 Reg = 0,0x00E2,0xA8 Reg = 0,0x00E3,0x00 Reg = 0,0x00E4,0x28 Reg = 0,0x00E5,0x38 Reg = 0,0x00E6,0x00 Reg = 0,0x00E7,0x00 Reg = 0,0x00F0,0x5F Reg = 0,0x00F1,0x55 Reg = 0,0x00F2,0x42 Reg = 0,0x00F3,0x39 Reg = 0,0x00F4,0x34 Reg = 0,0x00F5,0x39 Reg = 0,0x00F6,0x00 Reg = 0,0x00F8,0x00 Reg = 0,0x00F9,0x00
[REGISTERS] Device = ALP Nano 1 - DS90UB948, Connector 1 Comments = "Deser Device Data" Date = 07/08/2022 Time = 19:17:09 Reg = 0,0x0000,0x58 Reg = 0,0x0001,0x04 Reg = 0,0x0002,0x00 Reg = 0,0x0003,0xF0 Reg = 0,0x0004,0xFE Reg = 0,0x0005,0x1E Reg = 0,0x0006,0x00 Reg = 0,0x0007,0x1C Reg = 0,0x0008,0x00 Reg = 0,0x0009,0x00 Reg = 0,0x000A,0x00 Reg = 0,0x000B,0x00 Reg = 0,0x000C,0x00 Reg = 0,0x000D,0x00 Reg = 0,0x000E,0x00 Reg = 0,0x000F,0x00 Reg = 0,0x0010,0x00 Reg = 0,0x0011,0x00 Reg = 0,0x0012,0x00 Reg = 0,0x0013,0x00 Reg = 0,0x0014,0x00 Reg = 0,0x0015,0x00 Reg = 0,0x0016,0x00 Reg = 0,0x0017,0x00 Reg = 0,0x0018,0x00 Reg = 0,0x0019,0x01 Reg = 0,0x001A,0x00 Reg = 0,0x001B,0xF4 Reg = 0,0x001C,0x22 Reg = 0,0x001D,0x10 Reg = 0,0x001E,0x00 Reg = 0,0x001F,0x00 Reg = 0,0x0020,0x00 Reg = 0,0x0021,0x00 Reg = 0,0x0022,0x40 Reg = 0,0x0023,0x20 Reg = 0,0x0024,0x08 Reg = 0,0x0025,0x00 Reg = 0,0x0026,0x83 Reg = 0,0x0027,0x84 Reg = 0,0x0028,0x21 Reg = 0,0x0029,0x00 Reg = 0,0x002A,0x00 Reg = 0,0x002B,0x00 Reg = 0,0x002C,0x00 Reg = 0,0x002D,0x00 Reg = 0,0x002E,0x00 Reg = 0,0x002F,0x00 Reg = 0,0x0030,0x00 Reg = 0,0x0031,0x00 Reg = 0,0x0032,0x90 Reg = 0,0x0033,0x25 Reg = 0,0x0034,0x01 Reg = 0,0x0035,0x00 Reg = 0,0x0036,0x00 Reg = 0,0x0037,0x88 Reg = 0,0x0038,0x00 Reg = 0,0x0039,0x00 Reg = 0,0x003A,0x00 Reg = 0,0x003B,0x0F Reg = 0,0x003C,0x20 Reg = 0,0x003D,0xE0 Reg = 0,0x003E,0x23 Reg = 0,0x003F,0x00 Reg = 0,0x0040,0x43 Reg = 0,0x0041,0x03 Reg = 0,0x0042,0x03 Reg = 0,0x0043,0x00 Reg = 0,0x0044,0x60 Reg = 0,0x0045,0x88 Reg = 0,0x0046,0x00 Reg = 0,0x0047,0x00 Reg = 0,0x0048,0x0F Reg = 0,0x0049,0x00 Reg = 0,0x004A,0x00 Reg = 0,0x004B,0x00 Reg = 0,0x004C,0x00 Reg = 0,0x004D,0x00 Reg = 0,0x004E,0x63 Reg = 0,0x004F,0x00 Reg = 0,0x0050,0x03 Reg = 0,0x0051,0x10 Reg = 0,0x0052,0x00 Reg = 0,0x0053,0x01 Reg = 0,0x0054,0x80 Reg = 0,0x0055,0x00 Reg = 0,0x0056,0x00 Reg = 0,0x0057,0x00 Reg = 0,0x0058,0x00 Reg = 0,0x0059,0x7F Reg = 0,0x005A,0x20 Reg = 0,0x005B,0x20 Reg = 0,0x005C,0x00 Reg = 0,0x005D,0x00 Reg = 0,0x005E,0x00 Reg = 0,0x005F,0x00 Reg = 0,0x0060,0x00 Reg = 0,0x0061,0x00 Reg = 0,0x0062,0x00 Reg = 0,0x0063,0x00 Reg = 0,0x0064,0x10 Reg = 0,0x0065,0x00 Reg = 0,0x0066,0x00 Reg = 0,0x0067,0x00 Reg = 0,0x0068,0x00 Reg = 0,0x0069,0x00 Reg = 0,0x006E,0x00 Reg = 0,0x006F,0x00 Reg = 0,0x0070,0x00 Reg = 0,0x0071,0x00 Reg = 0,0x0072,0x00 Reg = 0,0x0073,0x07 Reg = 0,0x0074,0x07 Reg = 0,0x0075,0x08 Reg = 0,0x0076,0x00 Reg = 0,0x0077,0x00 Reg = 0,0x0078,0x00 Reg = 0,0x0079,0x00 Reg = 0,0x007A,0x00 Reg = 0,0x007B,0x00 Reg = 0,0x007C,0x02 Reg = 0,0x0080,0x00 Reg = 0,0x0081,0x00 Reg = 0,0x0082,0x00 Reg = 0,0x0083,0x00 Reg = 0,0x0084,0x00 Reg = 0,0x0090,0x00 Reg = 0,0x0091,0x00 Reg = 0,0x0092,0x00 Reg = 0,0x0093,0x00 Reg = 0,0x0094,0x00 Reg = 0,0x0098,0x00 Reg = 0,0x0099,0x00 Reg = 0,0x009A,0x00 Reg = 0,0x009B,0x00 Reg = 0,0x009C,0x00 Reg = 0,0x009D,0x00 Reg = 0,0x009E,0x00 Reg = 0,0x009F,0x00 Reg = 0,0x00C0,0x00 Reg = 0,0x00C1,0x00 Reg = 0,0x00C3,0x00 Reg = 0,0x00C4,0x00 Reg = 0,0x00C5,0x00 Reg = 0,0x00C8,0xC0 Reg = 0,0x00C9,0x00 Reg = 0,0x00CA,0x00 Reg = 0,0x00CB,0x00 Reg = 0,0x00CC,0x00 Reg = 0,0x00E0,0x00 Reg = 0,0x00E1,0x00 Reg = 0,0x00E2,0x00 Reg = 0,0x00E3,0x00 Reg = 0,0x00E8,0x00 Reg = 0,0x00E9,0x00 Reg = 0,0x00EA,0x00 Reg = 0,0x00F0,0x5F Reg = 0,0x00F1,0x55 Reg = 0,0x00F2,0x42 Reg = 0,0x00F3,0x39 Reg = 0,0x00F4,0x34 Reg = 0,0x00F5,0x38 Reg = 0,0x00F6,0x00 Reg = 0,0x00F8,0x00 Reg = 0,0x00F9,0x00
The technical specifications of one of the Laptop are attached below on which the problem is happening:

Please help me resolve this issue.
Thank you.
Regards,
Vikas