This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SN65DSI83-Q1: Can I use DSI83-Q1 and share the same PCB layout with DSI84-Q1?

Part Number: SN65DSI83-Q1

I am now working on a display project with two SKUs: single LVDS and dual LVDS and planning to use DSI84-Q1. However, I am wondering if could use DSI83-Q1 for single LVDS and DSI84-Q1 for dual LVDS which shares the same PCB layout? I knew DSI83-Q1's datasheet said RSVD pin should be "Reserved and leave them unconnected." Is it a must follow rule? Could I use the same PCB which only have the open stub on these reserved pin which used for DSI84-Q1?

Thank you.