This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DP83869HM: Termination resistor between SI_P and SI_N

Part Number: DP83869HM
Other Parts Discussed in Thread: DP83869

Hello

 

According to INF-8074 document, there is a 100ohm termination reistor between the SERDES IC pins, SI_P and SI_N.

Does DP83869 internally have this 100ohm termination resistor?

Is “Receiver differential input impedance (TYP:100ohm)” which is described on P12 of the datasheet same as this termination resistor?

 

Regards,

Oba