This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TSB81BA3 use of internal regulator clarification

Other Parts Discussed in Thread: TSB81BA3E

The data sheet mentions to tie VREG_PD to Vdd for normal operation of the TSB81BA3.  If I do that, I cannot use the internal 1.95V regulator and eliminate one extra part. 

The TESTM, VREG_PD, SE, and SM terminals are used to set up various manufacturing test conditions. For

normal operation, the TESTM and VREG_PD terminals must be connected to VDD through a 1-kΩ resistor. The

SE and SM terminals must be tied to ground through a 1-kΩ resistor. 

Can you please clarify how I can use the internal regulator to generate 1.95V if I need to tie Vreg_PD to VDD for normal operation?

Thank you,

Frank

  • Hello Frank,

    We are reviewing your inquiry, can you attach the document in which you are seeing that information regarding VREG_PD.

    Regards.

  • The TSB81BA3E can be powered by a single 3.3-V supply when the VREG_PD terminal (terminal 73 on the PFP

    package and terminal B7 on the ZAJ package) is tied to GND. VREG_PD enables the internal 3.3-V to 1.95-V

    regulator which provides the 1.95-V to the core.

    Datasheet for the TSB81BA3E, second paragraph in the Description section, page 2.

     

     The TESTM, VREG_PD, SE, and SM terminals are used to set up various manufacturing test conditions. Fornormal operation, the TESTM and VREG_PD terminals must be connected to VDD through a 1-kΩ resistor. The SE and SM terminals must be tied to ground through a 1-kΩ resistor.

    Datasheet for TSB81BA3E also in Description section, page 3, second to last paragraph.3252.tsb81ba3e.pdf

  • Hello Frank,

     

    Thanks for specifying that you are using the "E" version.

    You can tie VREG_PD to ground in order to enable the internal regulator.

    Please dismiss the "...for normal operation..."  paragraph.

    Regards.