Part Number: PCA9306
Hi experts,
PCA9306DCT apply for IBIS.
Apply for IBIS, Analysis using PCA 9306 DCT.
The analysis is performed using the following topology, but the waveform is not as expected.
Assumed waveform: High level rises to around 3.3 V.
Is it because the level conversion from 1.8 V to 3.3 V is not made?
Could you please confirm the following?
・circuit correct?(topology connection method)
・PCA9306_DCT setup (red) correct?
<files>
・PCA9306DCT_IBIS_Analysis_using.pdf
・IBIS : pca9306.ibs
/cfs-file/__key/communityserver-discussions-components-files/138/pca9306.ibs
Best Regards,
Takada