Part Number: TCAN4550-Q1
Other Parts Discussed in Thread: TCAN4550
Hi,
Case 1:
1. The bus is active with CANFD package is over 8 bytes
2. TCAN4550 is in standby mode, it is normal until 4 minutes passes. The abnormality is as below,

3. Even goes to normal mode, the fault doesn't disappear.
Case 2:
1. The bus is active with diagnostic package, 8 bytes
2. TCAN4550 is in standby mode, it is normal until 4 minutes passes, the abnormality is as below,

3. Even goes to normal mode, the fault doesn't disappear.
Case 3:
1. No package on bus
2. TCAN4550 is in standby mode and keep in silence for 10 minutes, it is normal.
My question is , why there is abnormality after 4 minutes in standby mode? Where am I wrong?
Thank you very much