Part Number: DP83867IS
Hi,
Just to confirm, is it possible to configure the CLK_OUT pin with 125 MHz without active link? The goal is to feed the MAC RGMII REF 125MHz input.
Thank you.
Regards,
May
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi May,
Yes it is possible to configure CLK_OUT to 125MHz without active link. However, just want to confirm you are not planning to use this as RX_CLK signal on the MAC, REF input is something different?
Thanks,
David
Hi David,
Just received update from customer, please see details below.
We are planning to use the CLK_OUT 125MHZ as REF CLK for the MAC. Could you explain the root cause of your recommendation. I would have the same concerns if we think about multiple PLL in series. PHY REFCLK 25MHz -> 125MHz PHY PLL CLK_OUT -> MAC 125MHz REF_CLK in -> MAC RGMII PLL ???. Is there a PLL involved in the RGMII MAC? I would expect all is clocked by 125 MHz.
PHY and MAC are running in the same 25MHz clock domain
Thank you.
Regards,
May
Hi May,
RX_CLK is part of the MII signaling and needs to have specific timing relationship to the RX_D0 - RX_D3 lines. CLK_OUT should not be used for this purpose.
However, it sounds like the REF CLK for the MAC is something different, so this should be fine.
Thanks,
David
Hi David,
Could you advise how to configure CLK_OUT 125MHZ without valid link? Customer guess its 125 MHz TX_CLK from internal 25 MHz to 125 MHZ PLL
Thank you.
Regards,
May
Hi Maynard,
You can configure the CLK_OUT pin in register 0x170.
The 125MHz CLK_OUT is generated by PLL from 25MHz reference clock, yes.
Thanks,
David