Part Number: IO-EXPANDER-EVM
Other Parts Discussed in Thread: TCA9539, TCA6424
I’m trying to communicate to the IO Expander EVM as a general I2C target to light up LEDs and I’m trying to do this without a MSP430 launchpad. I’m attempting to use the TCA9539 that’s on the board because it has more LEDs. However, I’m having some difficultly addressing it correctly.
I initially thought it might be the I2C host, but I can communicate to a different I2C target reliably so I think I have ruled that out.
My next thought is that I might have an incorrect setup for using the IO Expander EVM without an MSP430. The user guide is a little hard to follow. What jumpers do I need to connect to make the TCA9539 operate? I see that I may need to connect headers J9 and J10 but I’m not sure if this is for all 8-bit IO expanders or only a certain subset.
Alternatively, can you suggest another EVM that has a larger number (12+) of LED outputs with I2C communication?