Part Number: SN65DP159
HI team,
I would like to confirm whether the behavior that customer sees are correct or not.
HPD_SRC is affected by OE regardless of HPD_SNK status. Please see below.

Best regards,
Hayashi
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: SN65DP159
HI team,
I would like to confirm whether the behavior that customer sees are correct or not.
HPD_SRC is affected by OE regardless of HPD_SNK status. Please see below.

Best regards,
Hayashi
Hi Alex,
Can I confirm HPD_SRC = disabled means HPD_SRC pin is high-Z? Regarding the output type of HPD_SRC pin, is it open-drain or push-pull? Customer doesn't implement PU register at HPD_SRC but it works well, so guesses push-pull output.
Also the reported behavior is "OE is Low", will it be same in "0x03 bit3 = 0b" (power down by register)?
Regards,
Hayashi
Hi Hayashi-san,
You are correct. When HPD_SRC is disabled (Vcc<1.5V or reset) the pin will be high-Z. I believe it is push-pull output.
Low OE is the same as power down mode as you said. You can refer to this table for the different modes:

Regards,
Alex