Part Number: SN65LVDS100
Hi,
for specific applications, we have to eliminate any floating metal
I have very few PCB surface and I need to optimize qty of components
My goal was to connect the NC pin (pin 1) to VCC pin 8 (or GND or VBB)
can you confirm that this pin is not internally connected ?
if the pin is connected (biased) I could not need to connect it (can you give me details if it is the case)
Is it possible to get the internal metal surface in contact with this pin ? if very small we could probably left it unopened
thanks
Yves