Part Number: AM26C32
Hello All,
We are using AM26C32IPW RS422 Receiver ICs in our Design. As per my understanding, AM26C32 part has Fail-safe circuitry for RS422 inputs - Outputs of RS422 Receiver IC is High when there are no inputs at RS422 Receiver(Open/No driver condition/No cables connected).
In our Boards, when there are no RS422 inputs to this IC we have made some observations:
1. Some ICs outputs are low high and some are logic low.
2. In an IC, some 2 or 3 channel Outputs were low and One/Two channel output is High.
When we provide the right RS422 input signal, we get the right output. Whenever the IC inputs are open, we are facing issues. Please provide some suggestions/ideas for this issue (Can I provide an external fail-safe circuit).
We have terminated all the RS422 Reciever Inputs on our board using 100 Ohm Resistors.