Part Number: TUSB8042A
Hello.
Previously, we used one TUSB8042A Device to check the operation, and this time, we are going to check the operation using two devices.
I am writing because I have a question about clock input during the circuit configuration.
We are going to supply the XI input 24Mhz clock using OSC.
I wonder if it is okay to supply two TUSB8042A using one OSC operating at 1.8V.
Except for clock input, the remaining circuit diagrams copied the previously used circuit.