Part Number: TUSB8044A
Hello,
I have a new product in development and the customer have add the TUSB8044A USB hub to connect more devices on the USB host. On the third device is an STM32F205 with USB ORG FS only device connected. The USB communication between the STM32F205 and the USB host (PC) works without problems. But in the USB upstream I have many error frames with unknown type.
All other 3 downstream USB ports are not connected at the moment.
The error frames comes also when the STM32F205 is hold in power on reset. So I can say that this not come from my software.

How can comes this errors?
What can I do to remove this?
Thanks for Our help,
Bernd