This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TCA39306: Using the device for a switch during Vref1=Vref2 and Vref2 >= Vref1+0.7

Part Number: TCA39306
Other Parts Discussed in Thread: PCA9306

Hi INT team, 

I am designing with the PCA9306 or TCA39306 and I was curious about the switch/EN capabilities of the device. 

In the datasheet it calls out the Switch Mode vs the Translation Mode, but I wanted to know if you could also use the enable with a GPIO to open and close the switch. 

What I see in the other threads is to use an open drain GPIO connected at the VREF2 and EN pin. 

See diagram (should be an open collector npn BJT):

Will this work in both cases? 

I look forward to your feedback. 


Thank you, 

Mitchell