Part Number: DP83867IR
Hi,
I see below waveforms on TX and RX clocks when configured for 1Gbps. Can you confirm is this is acceptable?


This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: DP83867IR
Hi,
I see below waveforms on TX and RX clocks when configured for 1Gbps. Can you confirm is this is acceptable?


Hi Priya,
I have couple comments and questions on the scope snapshot. Here are the following comments and questions I have:
--
Regards,
Hillman Lin
Hi,
The connections that I have is - Ethernet switch --> Termination Resistor (0ohm) --> PHY Chip.
The switch is BGA package and I am not able to access the pin. The waveform I shared earlier is probed at the resistor end closer to the switch. The trace length between switch and resistor is 213mil.
I also probed directly on the TX_CLK pin on the PHY chip and it is not very different from the earlier waveform (RGMII2_TXC).
You are right that the rise and fall times are not compliant to the spec. The trace length between the resistor and PHY chip is 1990mil, which I dont think is much. The trace capacitance is ~6.5pF. The application note recommends to minimize the trace lengths below 5000mil.
I tried removing the termination resistor (basically disconnected the PHY) and probed the clock at the same resistor pad closer to the switch and the waveform improves significantly.
So its either the trace or the PHY chip itself loading the signal. PHY datasheet specifies input capacitance as 5pF. Are there any configuration settings that control the input slew rate?
Hi Priya,
Our PHY have a fix impedance on the MAC side. Here are the two possible solutions to fix your issue:
--
Regards,
Hillman Lin