Part Number: TUSB2036
We are having trouble getting our embedded hub design to function correctly. The design is meant to be used as an internal two port hub with one port always attached to a touch panel and the second an external slow speed device.
The schematics below have several errors that we have fixed:
- DP/DM swapped
- 48mhz crystal changed to 6mhz
- R1/R2 removed
- BUSPWR pulled high
- MODE pulled low

With these errors fixed and the board plugged into a windows PC, we get errors retrieving the device descriptor. A linux PC showed the same error.
The crystal only starts up when the device is plugged into the PC, then shuts off after a second or so (and the device has failed). We captured the USB trace on a cheap analyzer:
First group looks ok:

second does not:

We also noted that our crystal circuit does not have a 1.5K series resistor as in the EVM, but the signal levels look good at the IC.
Reset is generated by a voltage monitor - MAX811SEUS (140ms delay after VCC > 2.93V)
Any thoughts why this hub doesn't function properly would be appreciated.
Thanks!