Part Number: TCA9803
Other Parts Discussed in Thread: PCA9517
Dear Specialists,
We are planning to use TCA9803DGKR as below topology. We need your confirmation/suggestion. .
1. Connected the B side of TCA9803 to the I2C master device side and same net is shared to PCA9517(A Side)Level translator device which is 1.8V.
2.A side of TCA9803 to three slave devices are connected which is 3.3V logic.
3.B side of PCA 9517 is connected to four slave devices, which is 3.3V logic
Is it okay to connect multiple slaves in the configuration.
Could you please see the below configuration block diagram.

Please provide your feedback.
Thanks,
S.Satheesh