Part Number: AM26LV32
I would like to use this device in a circuit that can be driven by either an external differential driver or an external single ended driver. The single ended driver is TTL. If I bias the (-) input of the AM26LV32 to ~ 1.5V, and then wire the single ended driver to the (+) input and have it swing between 0 and 5V, it seems like I would get the correct output from the AM26LV32. Does that seem like a correct approach to making the AM26LV32 work for both cases?
Thanks,
Tim