Hi all.
I'm starting to work with ser/deser chips for the first time. I want to use it in conjunction with Chinese IPC camera chips. These chips only have one I2C port, which is used to control the image sensor. The question is, do I need to upgrade the image sensor driver in order to configure the deser chip first, and then transmit the image sensor control signals, or is there some simpler way. I don't want to rewrite the driver. The ideal option is to assemble the circuit, connect the deser to the ISP, the ser chip to the image sensor. Tell me the right way. Thanks in advance.