Other Parts Discussed in Thread: ISO1640, ISO1412, ISO1044, P82B96, ISO1641, ISO1540, ISO1540-Q1, ISO1541, ISO1541-Q1
Hello,
We have a product made up of one master unit connected by a cable to another slave unit. The communication is only I2C. The slave unit only has I2C peripherals with no CPU. The master has a CPU. The management likes me to use an optical cable (with as little quantity of fibers as possible) to have full isolation.
Do you have a solution to convert master side I2C to serial and to convert serial to I2C without any new software that needs to be developed? The closest I found is slaa908 (UART-to-I2C Bridge Using Low-Memory MSP430 MCUs) that does serial to I2C only.
The sloaa908 assumes the CPU is talking to the the serial side. This means in our master unit, we need to get the software person to rewrite the software to make all the code now talk to a new serial port. I would run the 2 optical lines to the slave unit. In the slave, I would have to add the MSP430F2311.
Or do you have any different ideas that involves no software?
Thanks,