Part Number: SN65HVD888
Hi colleagues,
Customer want test and verify VOH and VOL of SN65HVD888, can you show me the specific test circuit for these two parameter?
how to set the Peripheral circuit and adjust IOL(8mA or -8mA as show in DS)?

This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: SN65HVD888
Hi colleagues,
Customer want test and verify VOH and VOL of SN65HVD888, can you show me the specific test circuit for these two parameter?
how to set the Peripheral circuit and adjust IOL(8mA or -8mA as show in DS)?

This is a plain CMOS output, so nothing special is required.
Connect a 8 mA current/source between the output and GND/VCC, and measure the voltage. Alternatively, connect an ampere meter in series with a voltage source, and adjust the voltage source until you get 8 mA.
If you just want to check that the device meets the datasheet specifications, connect a 325 Ω resistor to GND or a 575 Ω resistor to 5 V (these result in an 8 mA load at the specified limits), and measure the voltage.
Hi Clemens, customer said when they test this 888 device whatever they put +200mV or -200mV at AB, the R always output high level, is the non-polarity feature cause that? and how can we modify the test circuit
Yes; the bus-polarity correction feature assumes that an idle bus is high.
To make the receiver switch low, you must input pulses shorter than tFS (44 ms).
Hi Stanley,
Clemens is correct here as well.
Please see highlighted line in datasheet excerpt below for polarity correction conditions:

As a note - this device is only setup to work with fail-safe resistors - if these are not included device behavior may not be consistent with expected results.
Best,
Parker Dodson