This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TCAN1145-Q1: Behavior as receiving FBFF or FEFF in sleep mode

Part Number: TCAN1145-Q1


Hi team,

My customer would like to confirm whether TCAN1145-Q1 is waked up as shown in "Frame error counter mechanism" of ISO 11898-2:2016, or not, when the device receives FBFF or FEFF.
Could you tell me the device behavior?

Best Regards, Taki

  • Hi Taki-san,

    TCAN1145 supports both standard IDs (11-bit FBFF) and extended IDs (29-bit FEFF). The low-power receiver is capable of identifying whether a received frame is formatted as either standard or extended formats and can be configured to wake on either format. When a frame is received with the format not used as a WUF, it will be ignored by the transceiver and will not generate a frame counter increment if the CAN frame is valid. 

    Let me know if you have any more questions.

    Regards,
    Eric Schott