Part Number: MAX3221
Hello,
I am looking for some help in determining if there is manufacturing differences between two of the same chips that were ordered at different times. We have an older version that works with our board, but when we purchased a new set of boards (outsourced board), the new batch has an issue with these MAX3221 and does not function as expected.
I have debugged the problem and narrowed it down to the MAX3221, in which changing out the component for an older component, the board functions as expected.
The MFR markings are as follows:
Working - "MB3221I 77AG3 P415"
Not working - "MB3221I 24KG4 A38E"
Are these different versions of the MAX3221? If so, is it possible to order the "Working" chips. The working chip is from an older board probably about 3 years old compared to the not working chip (<=1 month of having in possession).
Furthermore, if they are different, can you please let us know what the difference is?
Thank you!
Anthony J. Sanchez