Other Parts Discussed in Thread: SN75LBC180, SN55LBC180, SN65LBC180, P82B715, THVD8000
RS-485 トランシーバーの接続について質問です
I have a question about connecting the RS-485 transceiver.
御社トランシーバーの使用可否についての質問です
I have a question about whether or not your company's transceiver can be used.
住宅内配線再利用で複数制御基板の双方向通信を行います。
Two-way communication of multiple control boards is performed by reusing wiring in the house.
ただしラインが2本(1本は電源接続で使用)
However, there are 2 lines (1 line is used for power connection)
したがって信号は1本しか使用できません
Therefore only one signal can be used
SN55LBC180, SN65LBC180, SN75LBC180
イレギュラーな接続のため製品動作保証は不可であることは承知しています
I understand that it is not possible to guarantee product operation due to irregular connections.
Y,A端子でのみ送受信を行う
Transmit and receive only with the Y and A terminals
①IC Bの反転入出力端子とY,Aの入出力端子の間にインバータICを接続する。
(1) Connect an inverter IC between the inverted input/output terminal of IC B and the input/output terminals of Y and A.
受信時はインバータICからYの反転信号をBに入力させて動作させることは可能でしょうか?
Is it possible to operate by inputting the inverted signal of Y from the inverter IC to B when receiving?
②ZがオープンのままでもICは動作しますか?
(2) Does the IC operate even if Z is left open?
③最小の転送速度を教えて下さい
(3) What is the minimum transfer speed?
ノイズ悪化は許容します
Noise deterioration is acceptable
反射による波形劣化も許容します
Allows for waveform deterioration due to reflection
転送速度は低速に設定します
Set the transfer speed to slow
以上宜しくお願いします
Thank you very much