Part Number: DS90UB953-Q1
Other Parts Discussed in Thread: TDES960, DS90UB960-Q1, , TSER953
(Background)
We are currently in the process of selecting components for MIPI's FPD-Link III.
The required specifications for our products are as follows. On the TX side, 4 MIPI sensors are input to each serializers, converted to FPD-Link signals, and transmitted.
On the other hand, on the receiving RX side, the signals are input to 4-input FPD-Link deserializer hub, and then converted back to MIPI signals.
(Selected LSI)
TX side; DS90UB953
RX side; TDES960
(Contents)
The data sheet clearly states that the following sensor data output formats are supported. In particular, I have the impression from the text that it is stated with the nuance of "only this sensor output format can be used".
Q1) Can these LSIs transmit the sensor format "2560x1936@15fps MIPI;4(lane)"?
(Especially, It uses the same sensor and the same data format for all sensors.)
Q2) If the sensor is compatible with MIPI standard ver1.3, can we transmitted the MIPI signal by these LSI?