Part Number: DS125DF111
I have an application which uses (2) DS125DF111, one on each sides of a coax cable, in a 10GBE application. I want to set the DFE Tap 1 manually but when I do that the system does not link after bootup unless I go into the GUI and select the 'Device Status' tab and wait for an update. How can I set the DFE tap manually while still allowing the device to boot up and link correctly?