Part Number: TUSB320
Hi,
I would like to drive a small 12V motor through a 5V USB-C. The motor requires around 12V @ 0.5A to 1A i.e. max 12W which with 15W USB-C should be easily doable with a DC-Boost converter. I was thinking of using TUSB320 as a UFP CC-Controller to monitor the sources (DFP) capabilities. Additionally, I would like the chip to be able to interpret the BC1.2 standard however, I didn't find such CC Controller in your portfolio.
My questions:
- What DC-DC boost would you suggest with good efficiency for 5V to 12V conversion?
- Do you maybe have an IC which works as a CC-Controller and a DC-DC Boost?
- Which IC would you suggest for the protection solution of the USB-C?
- Maybe I wasn't looking well, but do you have a CC Controller which also works with legacy BC1.2?
Kind Regards,
Den