Part Number: DP83867IRPAP-EVM
Hi,
Can I know the bootstrap configuration to achieve 100 &1000 Mbps using DP83867IRPAPR?
Thank you
Regards,
Jeevan Sidharth G
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: DP83867IRPAP-EVM
Hi,
Can I know the bootstrap configuration to achieve 100 &1000 Mbps using DP83867IRPAPR?
Thank you
Regards,
Jeevan Sidharth G
Hi Jeevan,
Please see Table 6 in the datasheet. You can select the last option to achieve 100Mbps, otherwise any of the first 3 options will create a 1000Mbps link when connected to a compatible link partner.

Thanks,
David
Hi David,
Also whenever I set the speed to 100mbps, link up happens but the IP does not show up. When I try the same with 10 Mbps, it works fine.
Regards,
Jeevan
Hi Jeevan,
Please start a new thread and provide more details, since this is a new issue.
Section 8.5 of the datasheet has the pin names of the straps.
Section
Thanks,
David