Part Number: TLK10031
Hi
Now we have a TLK10031 connecting to a 10BASE-R SFP device
We test the Deep Remote Loopback mode and find the status PMA/PCS receive link up;but PMA/PCS fault condition is detected on tx path , so our connecting point (10BASE-R SFP point host computer)link down. The Flowing is our configuration and status register .How we debug the issue? Thanks
global reset"
"0x8610" > "0x401E0000"
#disable auto-negotiation
"0x2000" >"0x40070000"
#turn off lt_training
"0x0" > "0x401E0096"
#enable deep remote loopback
"0x0008" >"0x401E000B"
#link setting configured manually
"0x03FF" > "0x401E8020“
#HS_SERDES_CONTROL_2
"0x4848" > "0x401E0003"
#HS_SERDES_CONTROL_3
"0xD500" > "0x401E0004"
#data path reset
"0x0008" > "0x401E000E"
test result
CHANNEL_STATUS_1 value is 0x1c03
HS_STATUS_1 value is 0xf02b
HS_ERROR_COUNTER value is 0x00
---------------------------------
LS_CONFIG_CONTROL value is 0x371
LS_STATUS_1 value is 0x8000
LS_LN0_ERROR_COUNTER value is 0x00
LS_LN1_ERROR_COUNTER value is 0x00
LS_LN2_ERROR_COUNTER value is 0x00
LS_LN3_ERROR_COUNTER value is 0x00
---------------------------------
PMA_STATUS_1 value is 0x86
PMA_STATUS_2 value is 0xb800
---------------------------------
PCS_STATUS_1 value is 0x86
PCS_STATUS_2 value is 0x8801
KR_PCS_STATUS_1 value is 0x1005
KR_PCS_STATUS_2 value is 0x8000
---------------------------------
AN_CONTROL value is 0x2000
AN_STATUS value is 0x98
LT_TRAIN_CONTROL value is 0x00
---------------------------------
KR_VS_TX_CTC_DROP_COUNT value is 0x00
KR_VS_TX_CTC_INSERT_COUNT value is 0x00
KR_VS_RX_CTC_DROP_COUNT value is 0x00
KR_VS_RX_CTC_INSERT_COUNT value is 0x1185