Part Number: DP83848J
Other Parts Discussed in Thread: DP83848C
Hi,
I am using an Altera Cyclone III and trying to communicate with DP83848JSQ from an FPGA.
Even I did not plug the RJ45 jack of Altera Cyclone III to PC, the link up status always high. I have tried reading BMSR register. Here am getting 0x883a.
Do we have any specific configuration to initiate PHY?.
In my code, I have configured some control register bits. Those are below.
phy_cfg
{
BMCR 0x8000 (for self -clear)
ANAR 0x01E0
BMCR 0x1200
}
I have a register configuration profile for DP83848C & 78Q2120C (attached below), similar like do we have for DP83848J?
|
Ex: PHY Name : National DP83848C PHY OUI : 0x080017 PHY Model Num. : 0x09 PHY Rev. Num. : 0x00 Status Register: 0x00 Speed Bit : 0 Duplex Bit : 0 Link Bit : 0
|
"Teridian 78Q2120C", 0x39C, // OUI 0x0C, // Vender Model Number 0x9, // Model Revision Number 1, // Location of Status Reg 14, // Location of Speed Status 13, // Location of DuplexStatus 2, // Location of Link Status &teridian_phy_cfg, // Function pointer to &teridian_link_status_read |
And also question about the PHY TX_CLK and RX_CLK:
We have two boards, one has Teridian PHY IC another has TI PHY IC(DP83848J), I am able to get clock frequency from TX_CLK and RX_CLK pin on Teridian IC, but we didn't get signals when tested on TI IC(DP83848J). Please provide your comments.