Other Parts Discussed in Thread: DS90UB953-Q1, , TSER953, TDES954,
Hi,
We kick off a new project for the camera communicate with SOC(NXP I.MX 8 MX), and now we have below technology support need from TI;
1. We have below spec. for the camera:
1) Resolution: 1080*1280;
2) Frame rate: 100fps;
3) Color deep: 12bit;
4) Type: Black & White,
Please advise if the DS90UB954-Q1 and DS90UB953-Q1 are available or not for this reqest;
2. What the different between DS90UB954-Q1/ DS90UB953-Q1 and TDES954/ TSER953, and if we can dsign in same schematic diagram?
3. We will use the I2C to control the flash lamp , and now the I2C of DS90UB953 is control the image sensor, and please advise if we can add both image sensor and flash lamp mudule on the I2C bus parallelly;

4. We will design the schematic diagram same as the DS90UB954-Q1EVM, and please avise if we can use the crystal instand of the oscillator;

5. If we can use the internal 1.1-V regulator instand the TPS74801TDRCRQ1;
6. How to set the INTB? We have no idea what the situation we need to use the INTB;
7. We only have one camera(one MIPI) , and can we set the CLK0 or CLK1 to control the 4 lans for data transfer?
8. Please advise the BISTEN/ RSVD pin funcation and if we need to connect to GND as the EVM, thanks.