Dear TI Team,
It is seen that certain diagnostics tests do not function as intended.
1) Time Domain Reflectometry:
a) after performing TDR is activated by setting bit[15] in register 0x1E
b) wait 100ms
c) readback of 0x1e = 0x3 (Indicates TDR is completed but has faults), ideally it must be
0x2
d) readback of 0x310 = 0x0
2) BIST and loopback tests
a) MII loopback appeared to work ok, since as per register settings which are required to
be enabled Rx Cnt seem to be present after reading this registers: 0x063C, 0x063D, 0x063E
b) However Rx Cnt seemed to be zero for all the other loopback tests (which are also enabled accoring
to the spec); including PCS, Digital, AFE, Reverse Loopback
The MAC Controller is configured in RGMII mode, however I am not sure all the required register settings
for the PHY itself has been dp83tc812r configured.
Regards,
Annamalai