Part Number: TCAN4550
Other Parts Discussed in Thread: ISOW1044, ISO1042
Hi
Do you have any suggestions for substitutes with similar specifications to ADI ADM3057E OR ADM3050E?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Gareth,
Thanks for reaching out.
ADM3050E is an isolated CAN FD transceiver and the equivalent device from TI is ISO1042 while ADM3057E is an isolated CAN FD transceiver with integrated power and the equivalent device for this is ISOW1044.
If customer is using RI-8-1 package for ADM3050E then ISO1042 in DWV-8 package is going to be pin-compatible but RW-16 package of ADI is not pin-compatible to DW-16 package of TI. ADM3057E and ISOW1044 are also not pin-compatible. Let me know if you have any questions, thanks.
Regards,
Koteshwar Rao