Part Number: TLIN1021A-Q1
On testing TLIN1021AQ1 at Room Temperature in normal-recessive mode, transceiver is consuming current of 1.5 mA when supplied with voltage greater than 28 V to 36 V .The current consumed is greater than recessive current mentioned in datasheet (700uA) in normal mode. So please clarify on this current consumption .
Note : This Test setup has Connector Capacitor (100pF), LIN ESD Diode connected . LIN pin connected to the load of 550 Ohms /10nF and the transceiver is yet to be verified in Low and High temperature. Have also attached the datasheet value FYR.