Part Number: DS125BR111
Hi,
For SFI application, need series a capacitor as below?
If yes, any capacitor value is recommend? thanks!

thanks!
Jeff
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: DS125BR111
Hi,
For SFI application, need series a capacitor as below?
If yes, any capacitor value is recommend? thanks!

thanks!
Jeff
Hi,
If the DS125BR111 redriver is being implemented as part of an SFP module then the module board is required to implement AC coupling capacitors on the redriver high-speed inputs and outputs. If the redriver is being implemented on the system host board and interfacing to modules via SFI then the host board does not need to implement additional AC coupling caps on the SFI interfaces, as the module is supposed to have these AC coupling capacitors.
100nF is an adequate value for the AC coupling capacitors.
Thanks,
Rodrigo Natal