Hi,
Our customer is using TUSB3210 for PS2 to USB converter,
initially the PS2 lines (data and clock) were connected to the GPIO ports
Port 0(0.0 & 0.1), but there were issues like few keys on the PS2 keyboard doesn't work
properly or few keys echoed multiple times on the PC.
Meanwhile, these kind of issues were solved when the PS2 lines (data and clock) were connected to
Port 3(3.5 & 3.3).
This has solved the issue but I wonder what chould be the difference between these two ports
Port 0 & Port 3.
Looking into the datasheet, I can understand that Port 3(3.3) has "Input Port Interrupt"
function, but in our customer's application they are not using the Interrupt function and so
it won't make any difference between these two ports.
We have seen this behaviour with the TUSB3210 Generic EVM.
Please let me know if there are any comments on this issue.
Regards.
Paddu.