Other Parts Discussed in Thread: TPS2549-Q1, TPS2549
We have an application that requires a Samsung Tablet to run continuously at full screen brightness.
Although we only really need USB2.1 speeds, we need to draw approximately 1.6A - 2A from the USB port, while allowing data over the USB port.
Can anyone direct me to a chipset that would allow this? USB 3 speeds would be fine as well. I figure this would me implemented as a USB Hub that has hi-current capability, and which would draw the higher power from a separate power supply. What TI Parts would allow this?
Thanks!