Part Number: TLIN1441-Q1
Hi Expert,
Considering the functional safety requirement, customer have some questions when using TLIN1441-Q1 watchdog function.
The background is that customer use the pin mode for watchdog and choose the 40ms twindow(WDT connect to GND). Due to some limitation, the MCU can only generate the 25ms or 30ms watchdog signal.


- From the watchdog window timing diagram as above, the safe trigger area should 28±4ms, correct?
- The minimum and maximum value of twindow are 32ms/48ms, the minimum and maximum value of twdout are 16/24ms. Does this range include the accuracy of internal oscillator(±10%)?
- Customer decide to set the 30ms for WDI input signal watchdog cycle time. Is there any risk need to considered? Can some ESD or EMI events will have some influence on the correct identification of watchdog feeding?
Thanks!
Regards,
Ethan Wen