Part Number: TCA9617A
Hello,
Two question need your help:
1. What's the start point of IIC signa rise time ? A point or B point in figure 10?
or use the waveform no pedestal overshoot?

2. Usually, signal rise time is 10%--90% stable high level, is this definition also suitable for IIC signal? if not, please give me the corrective IIC signal rise time measure method.
base on follow AC and DC definition, it is 10%~90% rise time.


3. The third question is how to get VILMAX and VIH MIN value if we use TR and TF formula to calculate TR and TF? measure the actual waveform or quote from DC table VILMAX=0.8V, VIH MIN=5*1.05*0.7=3.675V?
Best regards
Kailyn