Part Number: SN65LV1224B
Other Parts Discussed in Thread: SN65LV1023A
Hello,
I have been doing a lot of testing with the MAX9205/MAX9206 and SN65LV1023A/SN65LV1224B SerDes LVDS pairs. When testing with the Maxim Integrated chips I was successful in achieving a steady lock signal (over 10s of hours without the MAX9206 !LOCK signal going logic HIGH) with different TCLK/REFCLK frequencies of 16.666, 20, and 25 MHz. I have been using the MAX9205EVKIT evaluation boards for my testing. Recently, I swapped in the pin compatible SN65LV1023A and SN65LV1224B onto the MAX9205EVKIT. I was hoping to take advantage of the lower minimum PLL frequency of 10 MHz offered by TI SN65LV1224B. It seems like the PLL in the TI part might operate differently? There is no change to my test setup yet I am getting bit errors and the !LOCK signal is going logic HIGH even at the lowest frequency of 10 MHz. The !LOCK signal worsens as I increase the frequency to 11, 12 13 MHz etc. It is unusable at the 16.667 MHz frequency which I previously had great success with on the MAX9206.
Was I mistaken to assume these are pin compatible?
I am providing a clean TCLK and REFCLK. I am using 10 m of Cat5e. Both these variables were identical when testing the MAX9205/9206 pair. Attached are some oscilloscope images. One shows infintie persistence while triggering on the TCLK signal. You can see that the TCLK has very little jitter and that the phase relationship of the LVDS differential data is constant and also has very little jitter. The solid blue bar is demonstrating that the phase relationship between TCLK and REFCLK is not constant. They are on seperate PCBs which are not synchronized, but this is okay and I was able to successfully transmit data with the MAX9205/9206 pair with the same setup. I am surprised to see that the PLL on the SN65LV1224B doesn't remain locked to this serial data. The second image is triggering off the !LOCK signal going logic HIGH.
Thank you in advance for you time and advice. Kind regards,