This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TFP410-EP: Dose TFP410-EP support the RGB444 and YUV422?

Part Number: TFP410-EP
Other Parts Discussed in Thread: TFP410

Hi team,

      Support need!

      My customer said that they wanted a device, the device is shown below

  1. DVP input and HDMI 1.4 output;
  2. Video format supports RGB444 and YUV422 output;
  3. supports audio output;
  4. Meet HDMI1.4b source certification;
  5. less than 16*16mm 

     1.  i want to recommend the TFP410-EP. Could you please verify this device could meet the customer need?  Do you have  better recommend? 

     2. what are differences between  TFP410-EP and TFP410?

YOURS

NAN